Back to Main Menu

Setting up single sign-on (SSO) using Microsoft Azure AD

Objective: Gain an understanding of how to configure SSO login to the Predictor Platform.

Authentication to Predictor Web App and Predictor Desktop via SSO is available for Microsoft Azure AD. In order to configure Predictor to allow for SSO login, users should first raise a support case by emailing ams-assetic-support.si@siemens.com

Azure Configuration:

Step 1: Azure server configuration:

Follow the Azure server configuration documentation to register an application for Predictor to integrate with: https://learn.microsoft.com/en-us/azure/active-directory/develop/quickstart-register-app

Step 2: Add 'User.Read' permission for the configured application in Azure, in the API permissions tab: https://learn.microsoft.com/en-us/azure/active-directory/develop/quickstart-configure-app-access-web-apis#add-permissions-to-access-web-apis 

  • Add permission grant “User.Read” permission to the application

     


Step 3: Configure the following Authentication URIs within Azure:

  • https:/id.eu.alm.siemens.com/login/callback

  • https://auth.brightlysoftware.com/login/callback

 

Predictor Configuration:

Preferred Method:

Step 1: Contact Assetic Support and nominate a user to be the Company Admin for Predictor. Support will then upgrade that user account to be the Company Admin.

 

Step 2: The Company Admin user can log into the Predictor Web App and select 'Profile Management' from the 'Profile and Settings' menu in Predictor, then navigate to the SSO config area in the Company Connection tab.

 

Step 3: Select ‘Microsoft Azure AD’ SSO type and populate the mandatory fields in the Company connection section, then click Save:

 

 

Note: Changing the 'SSO Type' back to 'None' will remove any SSO configuration, and authentication will revert to username and password.

Step 4: Field Mapping from Azure:

Field Name

Field Description

Value (Example)

Customer Email Domains

email domain

brightlysoftware.com

for email ‘john.doe@brightlysoftware.com’

Azure AD Server Domain

Azure server domain name

brightlysoftware.com

Navigate to Azure Active Directory → Overview → Primary Domain

 

Client Id

Azure Application Client Id configured for Predictor Application

Navigate to app registration menu → select the created application → overview


Client Secret, Expiry

Azure Application Client Secret and Expiry configure for Predictor Application.

Notes:

  • Note: The Secret Value is only visible on creation.

  • Expiry maximum is 2 years.

  • Once the secret has expired, the SSO connection will stop working. In future, Predictor will send a notification to the nominated company admin when this is about to expire.

‘App Registrations’ menu → select the created application → certificate & secrets)


Alternative Method:

If an organisation's IT team are unable to access Predictor Platform directly in order to complete the SSO configuration, the SSO details can be provided to Assetic Support via a secure method, and then these will be added into Predictor Platform by the Support team.

 

There are two options for the secure transfer of the SSO configuration details:

  • An organisation can send in a password-protected file. The file should be in the .json format and contain the following information:
    {
    "sso_type": "azure_ad",
    "client_id": "",
    "client_secret": "",
    "expire_date_utc":"2024-05-01T00:00:00Z",
    "client_server":"",
    "email_domain":""
    }
    Assetic Support will then add these details to the SSO configuration.
  • Assetic Support can provide a one-time use upload URL, which has a 3-hour expiry. This pre-signed URL is then used in an API tool such as Postman to securely pass along the SSO details to Assetic Support. To do this, Postman is used to make a PUT API call to the provided URL, selecting 'binary' and attaching a file containing the SSO details.
  • If successfully uploaded, the status code 200 will be received. If an error status code is received (4XX), a new upload URL will need to be provided.
    Once the file is successfully uploaded using the URL, Assetic Support will then add the provided details to the SSO configuration.

 

Note: After the SSO configuration process is completed, it will take around 5 minutes for the SSO login to begin functioning.